Network License Administration Guide
Note: This topic is intended for License Administrators and describes the process for setting up network-based licenses to allow multiple users (one at a time and at one site) to access a Keysight software license over a network server. Licenses are allocated in real time by the network server.
The process selected by Keysight for setting up network-based "floating" licensing uses a licensing service called FlexNet Publisher® from Flexera Software. The FlexNet service enables software licenses to "float" on a network server and not be tied to one specific computer. Network licensing involves a server-clientinteraction in which a client computer is required to check out a license from a server computer in order to access the software application (one license at a time and at one site).
Floating License Installation Overview
The process for installing a network-based "floating" license for a Keysight software application is summarized below. For detailed step-by-step instructions, see Installing the Floating License Server.
-
Go to http://www.keysight.com/find/floatinglicensemanager to download the files required to install and configure the Keysight Floating License Manager application.
- You will need to purchase a Software Entitlement Certificate for a floating license from Keysight. After purchasing the license, go to Keysight Software Manager (KSM) at www.keysight.com/find/SoftwareManager to redeem and install the license file on the server computer.
Note: If you are a first-time user of KSM, you will be required to complete a one-time registration on the web site. - If you need to manually install the Floating License Server, go to www.keysight.com/find/Keysight-network-server-software to download the component files required to install and configure the FlexNet license server. The files are contained within the LicenseServer.zip file.
-
Configure the license server using the lmtools.exe utility, which was one of the files extracted from the LicenseServer.zip file in Step 1 above. Using this utility, you will provide the directory path locations of the License Server Manager utility (lmgrd.exe), the purchased floating license file (*.lic), and the Debug Log file (*.log).
- Start the license server and confirm its status using the lmtools.exe utility.
- From the client computer, launch the Keysight application that will use the floating license. The client computer will establish a connection with the specified license server's vendor daemon (agileesofd.exe) and send a request for a floating license. The vendor daemon will check to see if any licenses are available and send a corresponding grant/deny message back to the client computer.
See Also
Installing the Floating License Server
Purchasing a Floating Software License